STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Intermittent weird text area

Hello.I try develop TouchGFX+FreeRTOS based project for my custom board.I have a text area problem. I attached photo. Also project attached.It is not stable. It looks like always updating.Also when i touch the buttons other text areas looks same just...

LCD.jpeg
Muharrem by Associate III
  • 1218 Views
  • 2 replies
  • 1 kudos

Resolved! adding external source file to touchGFX porject

Hi Team,"I'm working on a TouchGFX project that was generated using the TouchGFX Designer. I need to add source files for USB functionality. I tried adding the .c and .h files to the Core/Src and Core/Inc directories, but I'm getting an error stating...

usb prob.png
naveen by Associate III
  • 1225 Views
  • 2 replies
  • 1 kudos

Resolved! touchgfx error during generating code

Hi there,There is the following error in TouchGFX when I try to Generate Code, even for the previous projects that already generated code successfully. I uninstall and reinstall it and try other versions, but it failed again.  the message of the erro...

STjohn by Associate II
  • 4387 Views
  • 9 replies
  • 1 kudos