Skip to main content
rkhri
Associate II
October 3, 2018
Question

How to Set CUBEMX to Support LCD Display for STM32F469i-DISCO

  • October 3, 2018
  • 12 replies
  • 3051 views

Hello,

I am trying to set up CUBEMX so that it can support LCD display for the STM32F469i-Discovery board.

Unfortunately I had no luck in making the correct configurations to enable the LCD display or find an example project for the STM32 ac6 or maybe a .ioc file with LCD setings.

Is there anyone familiar with LCD on 

STM32F469i?

What are the correct configurations?

Thank you!

This topic has been closed for replies.

12 replies

ST Technical Moderator
October 4, 2018

Hello @rkhri​ ,

I recommend you to have a look at the examples provided in the STM32CubeF4 firmware package which can be a starting point to learn about programming and configure your application on SW4STM32 IDE:

STM32Cube_FW_F4_V1.21.0\Drivers\BSP\STM32469I-Discovery\stm32469i_discovery_lcd.c

STM32Cube_FW_F4_V1.21.0\Projects\STM32469I-Discovery\Applications\Display\LCD_Paint

STM32Cube_FW_F4_V1.21.0\Projects\STM32469I-Discovery\Applications\STemWin

You can find more details about LCD configuration provided in the AN4323 application note, section “How to use STemWin Library step by step�?.

I invite you to follow this FAQ : Create a basic Graphical Application using CubeMX

https://community.st.com/s/article/FAQ-STM32F746G-Discovery-Create-a-basic-Graphical-Application-using-CubeMX

Hope this helps you.

Kind Regards,

Imen.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
rkhri
rkhriAuthor
Associate II
October 4, 2018

thank's i too hope this

rkhri
rkhriAuthor
Associate II
October 4, 2018

but i programming in keil uvision

rkhri
rkhriAuthor
Associate II
October 4, 2018

can it be possible to give a finished project in MXCube under stm32f469? And if not difficult in keil with drawing just a line and a given background color!

rkhri
rkhriAuthor
Associate II
October 4, 2018

Please))))):downcast_face_with_sweat:

ST Technical Moderator
October 12, 2018

Hello @rkhri​,

You can get inspired from the examples available under STM32CubeF4 firmware package with Keil IDE: STM32Cube_FW_F4_V1.21.0\Projects\STM32469I-Discovery\Applications\STemWin\STemWin_fonts\MDK-ARM

Best Regards,

Imen.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
rkhri
rkhriAuthor
Associate II
October 15, 2018

Hi! this examples used GUI and BSP libraries. it's very hard code. For me very interesting standart examples code whith only standart HAL libraries. And this is examples without CubeMX examples!!!

Tesla DeLorean
Guru
October 15, 2018

While it might be nice to see CubeMX extrude a monolithic lump of code I somehow don't expect to see it happen.

There are a lot of inter-related things that must be set up properly for the whole to work, the BSP and component level abstractions make sense for ST, and CubeMX at some point might spit out some stitched together boiler-plate code in a similar fashion.

If you really need it to be just HAL code, and I think the BSP code uses HAL, you're going to have to cherry pick through the various components and stitch together a minimal monolithic source file. I think the interactions and interplay here are quite complex (CLOCKS, SDRAM, LTDC, DSI, etc), and it would cost a lot to provide it in that form.

Perhaps start with simpler projects that don't use the GUI, clone one of those and strip out the parts you don't need.

Perhaps the DMA2D or DSI examples

STM32Cube_FW_F4_V1.21.0\Projects\STM32469I-Discovery\Examples\LCD_DSI

STM32Cube_FW_F4_V1.21.0\Projects\STM32469I-Discovery\Applications\Display\LCD_DSI_ImagesSlider

STM32Cube_FW_F4_V1.21.0\Projects\STM32469I-Discovery\Applications\Display\LCD_Paint

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
rkhri
rkhriAuthor
Associate II
October 16, 2018

Thanks. you can, I'll be unbearable. Can someone give me an elementary example. the finished project in Keil which will include 1 pixel on this Board and the project in CubeMX from which the project was obtained in keil.

rkhri
rkhriAuthor
Associate II
October 16, 2018

all the examples I looked at, but I can not turn on 1 the pixel itself with an empty project