cancel
Showing results for 
Search instead for 
Did you mean: 

I do not enter in HSYNC interrupt DCIM STM32H743

esukh
Associate III

I want to fetch video data from camera via decoder (TVP5150AM1) through DCIM.

I configure decoder to output 4:2:2 8-bit YCbCr video with discrete synchronization and I do not get HSYNC interrupt,

DCMI->IER |= (0x1 << 4) | (0x1 << 0);

so, first time when I enter into the interrupt routine my DMA->NDTR register is already 0x0, what means that I filled up full buffer already, when I expect get HSYNC interrupt after ~760 data transfers.

What do I do wrong?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0