STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Incorrect color of standard buttons. png with transparent background. What is wrong?

Hi.The problem isThe project is in the memory of mcu (flash).button - OKThe project is in the memory of QUADSPI.what could be the problem?Добрый день.Проблема �?ледующа�?...Е�?ли пиши проект в mcu, отображает�?�? корректно. Е�?ли на флешку, то пропад...

0690X000009jsG9QAI.jpg 0690X000009jsGJQAY.jpg 0690X000009jsHCQAY.jpg 0690X000009jsHRQAY.jpg
lexabps by Associate II
  • 2638 Views
  • 4 replies
  • 0 kudos

Resolved! TFT ILI9341V 8080II mode with DMA.

Hello everybody,I'm developing a board with STM32F429 configured for a 8080II interface TFT display.I have a 240x320 TFT (ILI9341) and 5-6-5 frame buffer in internal RAM.Everything works and actually I flush the buffer on lcd via a loop that write at...

0690X000009jx9mQAA.jpg 0690X000009jx8oQAA.jpg
DVill by Associate II
  • 1847 Views
  • 2 replies
  • 0 kudos

ov9655 output format analysis

I capture an image using the ov9655 camera module. The selected the image format as rgb565. The image captured is getting captured clearly (as i can see it on the lcd). As a next step, I wanted to analyse how the image is stored in the camera buffer....

SPrak.4 by Associate II
  • 728 Views
  • 0 replies
  • 0 kudos

Dynamic create bitmap

I want to create bitmap dynamically. I called bmpId = Bitmap::dynamicBitmapCreate(800, 480, Bitmap::RGB565); I found bmpId is 0xffff.and then call Bitmap::cacheGetAddress(bmpId);system will dead loop in Bitmap::cacheGetAddress(bmpId);

DJin.3 by Associate
  • 1850 Views
  • 4 replies
  • 0 kudos

Camera selection and interface

HiWhat is the easiest way to interface a camera. AN5020 lists a number of camera sensors supported, however only the old OV2640 is included in the support packages.The most complex issue is setting up the sensor registers - do the manufacturers suppl...

pbayton9 by Associate III
  • 816 Views
  • 0 replies
  • 0 kudos