STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

How to set Display's parameters ?

In applications for STM32f746-disco board, the display's parameters in rk043fn48h.h are as the following:/** * @brief RK043FN48H Timing */ #define RK043FN48H_HSYNC ((uint16_t)41) /* Horizontal synchronization */ #define RK043...

0690X000009jrqBQAQ.png

Interfacing with hardware in TouchGFX Applications - Example ported to TouchGFX Designer V4.10 and STM32CubeIDE

Hello,I ported the first example in the article "Interfacing with hardware in TouchGFX Applications" to TouchGFX Designer V4.10 and then ported it to STM32CubeIDE V1.0.2.Please find it in attachment. I hope you find it helpful.I didn't use the ioc an...

Custom board

I have a custom board based on the H743Viit does not have external SDRAM but a QSPI flash for storage.My board has an external Video Processor with SDram connected by FMC-LCD-16bit interface.I would like to use TouchGFX , does it need the external SD...

stm32f779 hardware jpeg decoder no interrupts

Four months of trying to solve this on and off and still no closer to finding a solution.The 'JPEG_DecodingUsingFs_DMA' example works great on the stm32f769i-disco board but porting it to custom hardware and I never get an interrupt of ANY kind from ...

Keyboard implementation shows the correct image that is set as highlightBitmap when key is pressed, but pressing a key not always results in the buffer being updated.

EDIT - Solution was to increase key (hitbox) size, to prevent touch 'sliding' off the key before completing lifting of finger tipUsing the CustomKeyboard example provided with the TouchGFX designer v10 we have created our own implementation of the Ke...

EKlei by Associate
  • 1942 Views
  • 3 replies
  • 0 kudos

Resolved! Classes/functions to change the button graphics?

Hi, I'm trying to change the button bitmap from "button_pressed.png" to "button.png", after an interrupt event (without touching the display) . Could anyone shed some light on where I can swap the graphics? I'm a CPP novice, so the more information y...

kjtl by Associate II
  • 1525 Views
  • 2 replies
  • 0 kudos