STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Environment for using TouchGFX

I have been developing an application on an STM32H7 (on a NUCLEO-H743ZI board), using STM32CubeMX and SystemWorkbench/SW4STM32 on a MacBook Pro. I've been using an 800x480 Newhaven Display capacitive touch display (I ported their EVE2 library as best...

APagl by Associate III
  • 1267 Views
  • 1 replies
  • 0 kudos

Resistive Touch Solutions

Hi All,We are currently developing on the STM32H750B-DK platform. Our application is coming along and we are to the point we would like to layout a custom PCB based on the dev kit. We will be using a larger display and of course a larger touch overla...

belair55 by Associate III
  • 1119 Views
  • 1 replies
  • 0 kudos

Getting back into the loop!

Hi Everyone,Sorry for being quiet this past few weeks! I've been involved in doing some internal training and have had to focus on that. I'm gonna be spending some time starting tomorrow and going forward checking up on and answering every post that ...

Resolved! STM32F429ZE only has two options available (RGB666 and RGB565) in the LTDC configuration, there should be the RGB888 option according to the datasheet.

Hi, I'm not sure whether this is a bug in the Cube or whether I'm missing out something. I tried opening the F439 in the Cube and it has the 24-bit RGB option. Just to check while I was there I searched for the LTDC_B0 pin and found it on PE4, so I ...