STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! I was attempting to put a keyboard inside a modal window. When I run the simulator and try to open up my modal window I get "Assertion failed!... Cannot add Drawable multiple times"

void MainScreenView::setVacuumPositionPercentBoxClickHandler(const BoxWithBorder& b, const ClickEvent& evt) { // When target vacuum position box is clicked, display modal keypad with numericals targetPercentModalWindow.setVisible(true); targetPerc...

WLewe by Associate III
  • 2181 Views
  • 6 replies
  • 0 kudos

TouchGFX option stays disabled in STM32CubeIDE v1.1.0

I am creating a custom board project for STM32F769 in STM32CubeIDE v1.1.0 with TouchGFX support.Even after enabling CRC, LTDC, DMA2D, RCC, I couldn't get the TouchGFX option highlighted. I tried setting up QuadSPI and FMC SDRAM2 as per online tutoria...

gps by Associate II
  • 2414 Views
  • 4 replies
  • 0 kudos

STM32CubeMX, TouchGFX and Keil uVision integration problem

Hello,I am facing compilation problem in Keil when generating code from STM32CubeMX (choose GRAPHICS - TouchGFX) as follow:cannot open source input file touchgfx/hal/OSWrappers.hppAlso if I open the Keil code which generated from the TouchGFX then th...

R. by Associate II
  • 3377 Views
  • 6 replies
  • 0 kudos

How to develop an application with CubeIDE and TouchGFX using only flash memory and internal RAM with 8080 interfaced display.

Good morning everyoneI state that I am a newbie and have never used CubeIde and TouchGFX.We would like to develop an application using the CubeIde (gcc) and the TouchGFX at the same time.We would then like to use a processor of the STM32L4 or L4 + fa...

Alberto1 by Associate III
  • 2964 Views
  • 7 replies
  • 0 kudos

Stm32f746IG interfacing with ADV7180 camera driver

I have taken a sample camera code of stm32f756 eval board in which the camera driver ic was S5K5CAG.and interfaced the dcmi peripheral and i2c configuration peripheral but i am unable to display camera output on the LCD display. I am using ADV7180 ca...

Uc.2361 by Associate II
  • 1144 Views
  • 1 replies
  • 0 kudos

Code diferences between IAR and Touchgfx

Hello, I have a touchgfx project. When I compile project with touchgfx IDE (with Run Target button) It works properly. After that I open IAR IDE, compile and flash to my board but it doesnt work properly. When I debug software, I see there is a hard ...

Epamuk by Associate III
  • 1308 Views
  • 4 replies
  • 0 kudos