STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Fonts visualization in designer

HiJust started to use the TouchGfx, notice an issue with fonts in the designer.I added a new typographies for a font i want to use in a new project, up to this part no problems. But when introduce a text area in the designer and select the new font, ...

0690X00000AsPPYQA3.png

Resolved! How to use Touch GFX on mac

I'm new in stm and i am using mac os and stm32cubeide for maci know touch gfx is not getting on mac nowi wonder how can we use touch gfx on mac?So the only way is installing window?Thanks

SKim.1761 by Associate III
  • 2482 Views
  • 1 replies
  • 1 kudos

TouchGFX 4.12 Can't Add Image

Hello,I am using TouchGFX 4.12. Here is what i have done and what is the problem;Created new project from CubeMX.Enabled TouchGFX from CubeMX.Opened TouchGFX and added a image object.Imported png images to the project path via image object's image pr...

Resolved! STM32F401RE Hangs working with 1BPP

Hi, TouchGFX communityI'm trying to get TouchGFX working on a STM32F401RE device with a 200x200 screen.I've created a simple project with one screen and text as 1bit color depth (Idither_algorithm := 2, opaque_image_format := BW, non_opaque_image_fo...

ADC Configuration & STemWin configuration bugs in MX Perspective and CubeMX Version: 5.4.0 Build: 20191009-1541 (UTC)

There is a bug in ADC configuration (MX perspective): "DMA Continuos Conversion Request" cannot be selected. And is rewrited back to disabled with code regeneration when corrected in code by hand.There is a bug in STemWin configuration (MX perspectiv...

RaJa by Associate II
  • 654 Views
  • 0 replies
  • 0 kudos