2019-07-15 1:11 AM
Hi @Martin KJELDSEN !
You usually support me with TouchGFX, this must be a simple one for you but I can't find the solution in the community.
I'm having an issue trying to update my project from TouchGFX 4.9.6 to 4.10. I get the build error:
undefined reference to `touchgfx::HAL::copyFBRegionToMemory(touchgfx::Rect, unsigned short*, unsigned long)'I think it is because I miss the function copyFBRegionToMemory(touchgfx::Rect, unsigned short*, unsigned long) in \touchgfx\touchgfx\framework\source\touchgfx\hal\HAL.cpp. Where can I find the latest version of source code to update?
Solved! Go to Solution.
2019-08-05 5:16 AM
Hi @Sandy.Dahl,
Back from vacation. There's just one version of 4.10.0 and the signature for copyFBRegionToMemory() hasn't changed.
Did you figure anything out while i was gone?
/Martin
2019-08-05 5:16 AM
Hi @Sandy.Dahl,
Back from vacation. There's just one version of 4.10.0 and the signature for copyFBRegionToMemory() hasn't changed.
Did you figure anything out while i was gone?
/Martin
2019-08-06 11:57 PM
Hi Martin!
I didn't figure out why I got that error. I deleted the TouchGFX-lib (4.9.6) and added 4.10 again, and the error somehow didn't return! So the issue is solved.
Thanks!
2019-08-07 12:42 AM
Okay, that's great :)
/Martin