STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Image add problem for version 4.12.3

Hi,I am try adding image on my application with new TouchGFX Designer version. I added image in assets file in project. I can see added image to "Images" tab. But I can't see anything in project tab of widgets image selection.How can i solve this pr...

0690X00000Aqd3XQAR.jpg

Clicked and released signal from the same button

In TouchGFX it is possible to call a C function when a flexi button is clicked (Trigger "touch") or released (Trigger "clicked").Is it possible that the same button calls an "I_m_pressed()" function when you stay button clicked AND sends an "I_m_rele...

Long rendering time when moving two images

Hi @Martin KJELDSEN​ On a screen I want to move two large images (one has transparency). I've implemented it like in your birdgame example (with the moveto(x,y) method.Now I recognized that the animation is very slow and the rendering time is very lo...

Marco.R by Senior
  • 4966 Views
  • 14 replies
  • 1 kudos

Adding Touchgfx remove code for Timer3

Hi,I am using STM32F778AI and I use PC7 as PWM generation . When I added TouchGFX it stopped generating code for Timer 3 and if I remove Timer 4 it cannot be added with the same reason.Any help ?Thanks!!David

davidra7 by Associate II
  • 914 Views
  • 0 replies
  • 0 kudos