User Activity

Hi ST-Community,I already set the speed of the scrollable container to maximum via calling of the function setMaxVelocity(0xffff).But I'm still not satisfied with the actual scroll speed.is there any other possibility to increase the scroll speed?BRD...
Hello,i use a custom DSI display on the STM32F769 Discovery Board.The display has 720x720 pixels and no framebuffer. Therefore I can't use the DSI adapted command mode but I have to use the DSI video mode.I have the following problem:When the pixel c...
Hello,i have 25 MHz HSE Clock.The DSI PLL settings are as follows: IDF 5, NDIV 80, ODF2With these settings i measure an DSI clock of 100 MHz on the DSI_CKP pin.But Cube says that the DSI clock is 200 MHz.I use a STM32F769NI device with 2 DSI data lan...
Hello,when I run the code with the STM32F769 discovery bord display, everything works fine.But when I use a differnt display the constructor for the start screen is not called from touch gfx lib. Does anybody know why this is only working with the di...
Kudos from