STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Avoiding snprintf

Is it possible to avoid using snprintf in TouchGFX. Is there any alternate method available to copy values in the buffer and display it without using snprintf.

PBU by Associate III
  • 2503 Views
  • 6 replies
  • 0 kudos

JPEG Codec Decoding Stock!

Hi all,I`m trying to decode jpg with JPEG Codec, and I reference the sample code from CubMX Official code { JPEG_DecodingUsingFs_DMA }, then inserted to my code.And now it stocks in this function:do { JpegProcessing_End = JPEG_OutputHandler(&...

I'd like to give my users the ability to chose skins at run-time. Is there a way to divert the calls to get button images from internal/external FLASH and load them from the an external source like an SD Card?

I'm pretty new to STM32 & TouchGFX. I'm building a device based on the STM32H743 with 8MB SDRAM & either 64 or 128MB QSPI FLASH. I will also embed a 2GB uSD card for extra storage.My initial idea is to have a few skins available and stored as extra d...

JimFouch by Associate III
  • 1242 Views
  • 2 replies
  • 0 kudos

Resolved! Weird behavior when animation

Hi,I'm working with TouchGFX with STM32F746BG, and I have an issue when there is animation.You can find a video of the problem here : https://youtu.be/X-D-NkGCN5kI also have the same issue when I add an animation between screen.At the beginning I was...

vtunr by Associate III
  • 3999 Views
  • 13 replies
  • 0 kudos

HardFault with very basic TouchGFX application

Hello everybody,I created a simple application with TouchGFX Designer (4.12.3) (a screen with a central button). My target card is SMT32h743_EVAL2 and the toolchain used is Keil uVision (5.28.0.0). I tried to load the compiled application using Keil...

ECiav by Associate II
  • 2137 Views
  • 3 replies
  • 1 kudos