STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Strange problem with STemWin Library

Hello everyoneI'm working on STemWin532 library on STM32F103ZET6 bord in STM32CudeIDE. I could successfully configured LCD interface (The Controller is HX8325B and GUI runs on internal RAM) and insert some text on the screen (following image):But whe...

0693W000000VhwFQAS.png 0693W000000VhwKQAS.png 0693W000000VhwAQAS.png 0693W000000VhwUQAS.png
Ahaji.1 by Associate II
  • 834 Views
  • 0 replies
  • 0 kudos

Resolved! Animated image - update interval issue with RTX5 RTOS

Hi,I am building a "cross-IDE" project with a bunch of different tools. That is why I have either FreeRTOS as well as Keil RTX5 RTOS in my project. I can switch between both kernels at any time.The problem I have regards animated image and it is inte...

aroni525 by Associate II
  • 1954 Views
  • 2 replies
  • 0 kudos

Resolved! Change the pixel (0,0)

Hello,I developed an application in touchgfx and it is working perfectly.It is 480x800 resolution and the display is oriented in landscape mode.When I installed the display in the device I realize that the base only fits in one way and therefore the ...