STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

I have a project to display some text using touchgfx. I'm using a custom H750 board, a LCD-TFT display. My LTDC, DMA2D, SPI is working fine but when i try including touchgfx, every time the framebuffer gets zero.

 I'm not using rtos, my touchgfx process is included in while(1). After debugging through IAR, i've run it and below image is from the .map file. I've also checked the memory address, it is getting zero only.

0693W000000WouwQAC.png
biki by Associate II
  • 4966 Views
  • 10 replies
  • 0 kudos

Resolved! Automate make command in Touchgfx environment.

I want to automate the process of "make" command using a batch file or whatever way convenient. Is it possible to send command to touchgfx environment using batch script ? Or write a batch script in touchgfx environment.

FShai.11 by Associate II
  • 1641 Views
  • 3 replies
  • 0 kudos

Problems using Touch GFX with STM32F469I-DISCO

Hello Everyone,I just got a F4 DISCO board after seeing the webinar on touch gfx and playing around with the designer but I am having problems uploading my design to the board. The screen is completely blank. I found couple articles for using CubeMX ...

If UART buad rate < Data rate from camera,there will be data losses, but Is it a problem if UART baud rate >data rate from camera?

I have an OV7670 interfaced to a nucleo board. Frame rate=10fpsImage format= qcif(174X144) ; YUV422(monochrome only)Pixel clock =8MhzSuccessive bytes of a row(Line) ,arrive at the rate of 8M bytes/sec, which is too high to directly transfer the incom...

Sprat.1 by Associate II
  • 3253 Views
  • 7 replies
  • 0 kudos

did the future version of STM32CubeMX support STemWin?

Hi guys,I'm very like the developing tools ST provided, and I feel ST have a good vision of what kind of resource will be needed by users.Recently, I'm building a product with TFT-LCD and I picked STemWin as the graphic library going to be used by ou...

JWu.2 by Associate II
  • 2325 Views
  • 3 replies
  • 0 kudos