STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! can TouchGFX support STM32H750VBT6 ?

It have a new project with LCD(4.3' RGB:480*272) and touch panel, To drive this LCD and touch panel, i will select STM32H750VBT6 to develop , Whether can the TouchGFX support this MCU or not ?

miker by Associate III
  • 2385 Views
  • 6 replies
  • 7 kudos

Issue Importing Images into TouchGFX

Hello,I am trying to import several images into my TouchGFX assets. I'm able to load them in and build, but when I flash my application hard faults. I've noticed the error once I exceed ~8Mb in the external flash.I believe I should have 64Mb of exter...

mmautient_0-1749214631320.png

Resolved! Framebuffer in PSRAM on STM32N6570-DK

Hi,I have created a simple GUI using TouchGFX Designer for the STM32N6570-DK, generated the code, built it, and ran it. Everything works fine.Then I noticed that the TouchGFX_Framebuffer is located in internal SRAM. However, I plan to use that SRAM f...

ERROR by Senior
  • 3038 Views
  • 9 replies
  • 0 kudos