Skip to main content
Junde
Senior III
September 29, 2024
Solved

How to rotate the image in TouchGFX?

  • September 29, 2024
  • 3 replies
  • 1604 views

Hi there,

In my STM32F429BI TouchGFX project, I using some images.

I want to show a image in areaA, and then rotate the image 90dgr and show it in areaB.

But seems I must store the 2 images(before and after the rotation) in RAM to show both of them.

Can I just store one image, and rotate the image by some setting to save the memory?

Thanks for your help!

This topic has been closed for replies.

3 replies

Junde
JundeAuthor
Senior III
January 9, 2025

Does the TouchGFX NOT support this function?

If yes, how about adding it?

unsigned_char_array
Lead III
January 10, 2025
"Kudo posts if you have the same problem and kudo replies if the solution works.Click ""Accept as Solution"" if a reply solved your problem. If no solution was posted please answer with your own."
Junde
JundeAuthor
Senior III
January 13, 2025

@unsigned_char_array 

Thanks for your information!

I tried Texture-Mapper, and it works well.

It's just a bit too powerful for my needs, especially since I only want to rotate an image 90 degrees.