User Activity

hello,I customized a board with stm32h743iit6 for HMI application, the main hardware features available on the board are RMII ethernet, 32bit SDRAM and LTDC RGB565 interface. Below is the board picture.A test MDK keil project is generated by cubemx t...
hi,    Recently I notice that toucgfx simulator screen size is twice the value set in toucgfx designer, if I want the exact pixel size set in touchgfx designer while simulating, is there a scaling factor or some function to call? thanks for your time...
Hello,I'm working on a vt100 terminal emulator,  so I created a custom widget which decodes input stream and then display it on a TFT-LCD by LTDC. It works fine alone,  after a custom keyboad added on the top, the simulation will crash when the custo...
Kudos from