STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! How to write a monospace (fixed-width) string to LCD?

Hello, I want to write time on LCD in format 00:00:00 (hh:mm:ss). I use simple text area object and font I use is Proxima Nova Semibold. But the problem is that text is moving around because each char have different width. I would like to each char s...

EPois.1 by Associate
  • 2017 Views
  • 3 replies
  • 0 kudos

Trying to generate keil project from Touch GFX

Hello.I am building a GUI for STM32f769 discovery baord on touch GFX . But every time when I generate the code, only EWARM and a Cube Mx project is being generated. At the other hand, On touch GFX website, It is mentioned that It can generate the c...

Kylo Ren by Associate II
  • 1448 Views
  • 2 replies
  • 0 kudos

TouchGFX in custom board configuration without CubeMx

I'm using Keil directly to STM32H7 with CMSIS core and Device startup only (without HAL). The inits & peripheral usage has implemented directly to registers.Is there any way (documentation/API?) connect to TouchGFX, when functionality is implemented ...

Kura by Associate II
  • 1452 Views
  • 1 replies
  • 0 kudos

is there any video tutorial for F469 discovery board ?

I see that there is integration with Cube IDE and Touch GFX. But I need to figure out how to set it up. I see a lot of demos showing the fancy graphic but it is usless if nobody shows how to actually write the code. I see a lot of people get discour...

MNapi by Senior III
  • 9668 Views
  • 27 replies
  • 0 kudos

Resolved! 7 or 8 Inches display on custom board based on F746

Hello,On a custom board (similar to F746-Disco board) i was able to setup a 5' display with 800*480 resolution on RGB565.Now, i would like to support bigger display with same board. As i checked, there are many 7+ inches displays with RGB interface.I...

0693W000001sWLmQAM.png
SKokk.1 by Associate II
  • 1564 Views
  • 1 replies
  • 0 kudos

Porting TouchGFX - can't write to screen

Hi everyone!I'm trying to port TouchGFX over to the CoreH743I board and I'm running into some trouble at the step of trying to write to the screen from main memory.https://support.touchgfx.com/docs/development/board-bring-up/how-to/03-display-interna...

GGowi.1 by Associate II
  • 1802 Views
  • 2 replies
  • 0 kudos

Two problems porting TouchGFX to CoreH743I - missing LTDC_IRQHander() and a HardFault during HAL_Init().

Hi,I'm trying to port TouchGFX to the CoreH743I board and I'm following the instructions on how to do that. In part 3 on bringing up the framebuffer I'm running into two problems:The internal CubeMX in CubeIDE is not generating the LTDC_IRQHander() f...

GGowi.1 by Associate II
  • 3025 Views
  • 8 replies
  • 0 kudos