STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

STM32f469I-Disco: PA11 and PA12 not working for CAN1

I am using STM32F469I-Disco board. Now, I am trying to use CAN1 and want to display messages on display using touchGFX. Now the main concern is, the only available CAN1 pins on this board are PA11 and PA12 and I tried and read that those pins are ass...

NTriv.1 by Associate
  • 1501 Views
  • 1 replies
  • 0 kudos

Rendering time issue with screen transition

Hi,I am working on STM32L4R9 Discovery kit and STM32L4R9 Evaluation kit , which has the 390x390 display.I have created a simple project with 2 screens one is with analog clock and two buttons and another one is just with an image. Whenever screen tra...

Bala1 by Associate II
  • 2633 Views
  • 5 replies
  • 0 kudos

Resolved! Hello, I am working with CubeIDE 1.3.1 and TouchGFX 4.13.0. I have to move my project on an other computer, but this version of CubeIDE is not available on ST web site now. Do you know where I can download CubeIDE 1.3.1 again ? Thanks a lot

 On the ST web site, there are CubeIDE 1.3.0 and 1.4.0, but both have some issues with TouchGFX : the first one is too old for TouchGFX, and for the other, TouchGFX is too old.For more details and if I understood well : TouchGFX generate a CubeMX pro...

GMich.2 by Associate II
  • 3167 Views
  • 5 replies
  • 1 kudos

STM32F746G-Disco as HID keyboard

Hi,I would like to make an application that simulates a keystroke when I press a button.I have configured my project as shown in this article and have tried the given code to simulate a looping "hello world" message keystroke but cannot get it to wor...

ETH is not working when integrating LWIP with LTDC

We are using STM32F429IGTx microcontroller for our application. We use STM32CubeMX with Keil IDE v5. Our application needs both LCD and internet connectivity. we try to use 800 x 480 TFT LCD ( RGB565 ) for display and ethernet for internet connectivi...

S_1 by Associate III
  • 5248 Views
  • 5 replies
  • 0 kudos

Resolved! Custom Project for H750-DK board from cubeide and touchgfx get stuck in __ExtMem_Boot_bin_Start()

HI,I am trying to create a touchgfx application project from cube ide for H750 board. I was able to get everything compiled after merging lot of things from the project created from touchgfx it self for h750 board. But once i run my custom project, i...

0693W000003BHEnQAO.jpg