STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Touch GFX and touch api issue

Hi,i'm trying to use a touchgfx with a capacitive touch. I have wrote a simple demo example. During the simulation i can switch an on / off a switch button just clicking with the mouse on it.In my hw integration i'm using the sampleTouch to give the ...

TomJJJ by Associate II
  • 3007 Views
  • 4 replies
  • 0 kudos

TouchGFX modelListener handling in Model::tick()

Hi,I'm trying to make an simple TouchGFX application that update a TextArea. But when i try to call, from Model::tick(), the modelListener pointer and access to the ViewPresenter function, it is not available. So i have probably misunderstanded some...

Woula by Associate II
  • 1640 Views
  • 1 replies
  • 0 kudos

LCD.blitCopy parameters.

Can anyone explain to me what the parameters to LCD.blitCopy are?The online help seems to suggest all of the parameters describe the source - sourceData, sourceFormat, source and blitRect all describe the source data. How do I specify the destinatio...

FTkal.1 by Associate II
  • 1758 Views
  • 4 replies
  • 0 kudos

Dear ST Community, i tried sometimes but still unsuccessful. can you all provide the STM32H750B-DK , with toughgfx step by step how to set by STMcubeMX, and compile ,programming, verify,debug by Keil procedure. Just want download simple image and run it .

Dear ST Community, i tried sometimes but still unsuccessful. can you all provide the STM32H750B-DK , with toughgfx step by step how to set by STMcubeMX, and compile ,programming, verify,debug by Keil procedure. Just want download simple image and run...

KLau.1 by Associate II
  • 3805 Views
  • 8 replies
  • 0 kudos

MoveAnimator setMoveAnimationEndedAction issues

I am trying to set a callback function for a container in motion using setMoveAnimationEndedAction . Can I only use this functionality from within a container?I have created a custom object that has a member variable Container which is utilizing the...