User Activity

I have the library installed, the application selected, and the selection under Additional Software X-CUBE-TOUCHGFX... selected and enabled. However, when I hit Generate Code, none of the TouchGFX folders are created, and the build fails with missing...
We have a custom board based on the 32H743IIT and I'm trying to do board bring-up and get TouchGFX working. We're using TouchGFX Designer 4.13.0, CubeMX 5.6.0, (updating to 5.6.1), and Keil uVision 5.29.0. I'm trying to follow the information on htt...