STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

F429 TouchGFX not working on own PCB

Hi! I have a program with TOUCHGFX running on F429-DISC1. It works fine and display correctly both on the disc1 original touch screen and an external screen with RGB666 interface i connected to the header.​As it look alright on the DISC1 board, i mov...

Resolved! System Requirement for TouchGFX on STM32F303xx

I am using STM32F303VBT6 in my application where I need to use the graphical library for advanced HMI development. The system would have more than 15 screens (consists of Text, symbols, images etc.), LCD is not a touch display it is simple 262K color...

Resolved! My TFT display looks ok, but after adding code to my project, not related to the display driver, the screen output is skeewed / Distorted. Need help thinking

HW setup is a self built board using the STM32H743V MCU and a Sharp LQ104V1DG61 TFT display. Display is setup to L8 and using CLUT table, Running on 25MHz (measured) it has a 640x480 format, RGB666 (yes I know that is not part of the supported format...

Zainka by Associate III
  • 4658 Views
  • 8 replies
  • 0 kudos

Resolved! How do I use hardware buttons (e.g. wakeup, joystick, and/or tamper buttons) as triggers to interactions using TouchGFX Designer on a STM32F469I-EVAL evaluation board?

I'm using TouchGFX Designer 4.15 with a STM32F469I-EVAL evaluation board. I'd like to use the hardware buttons on the eval board as [physical] inputs to control actions on the touchscreen display.

MBaum.2 by Associate
  • 1497 Views
  • 2 replies
  • 1 kudos

Resolved! [TouchGFX] How to zoom on a Shape

Hello,I'm currently developping on a STM32H7 with TouchGFX library and I'm wondering how to zoom on a shape created with touchgGFX designer ?The problem is that I'm using setPosition function to increase width and height and to change X and y positio...

AJT by Associate III
  • 1978 Views
  • 3 replies
  • 0 kudos

Resolved! Missing functions in generated code (TouchGFX 4.14)

Dear ST community,I am trying to build a basic test project for the STM32F469I-DISCO board, using STM32CubeMX 6.0.1 and TouchGFX 4.14. The generated project code fails to build because of a number of absent function implementations. Details below.Ste...

villains by Associate II
  • 2132 Views
  • 2 replies
  • 0 kudos

Resolved! Changing color of the circle using physical button

Working on designing the GUI in such a way that need​ to change the color of the small circle to indicate the status and also to show the mode changes . If one mode is selected circle color should be green or else white ....... im trying to work on t...

KM L.1 by Associate II
  • 3066 Views
  • 6 replies
  • 0 kudos

STM32H747 MIPI DSI Command mode

HI ST,I do a project about MIPI DSI but have an issue: when send the first command DSI in command mode, status is HAL_OK and I see the signal on scope (DSI D0P/D0N). After that, Pin DSI D0P/D0N is in level 0 and don't send the next command.DSI Confi...

NHo.1 by Associate III
  • 1404 Views
  • 1 replies
  • 0 kudos