STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

[STM32F769] Hang-up inside setLanguage function in flashing(burning) mode, but working ok in debug mode.(with flash : M29W128GL)

My board(custom board) hang-up while init(setLanguage function) after burning image to flash. In debug mode(debug->run target), board is working ok. Here's the hang-up point://Texts.cppcurrentLanguageIndices = staticLanguageIndices[id];sprintf(dbgbuf...

Phyo .1 by Associate II
  • 1174 Views
  • 1 replies
  • 0 kudos

A question about creating a screen menu system

I am trying to make a menu screen system which I thought first would be trivial, but until I figure it out it isn't... There are radio buttons for selecting the wanted measurement and a start button. The idea is to send the chosen test ID to the Mode...

HHarj.1 by Senior
  • 2816 Views
  • 5 replies
  • 0 kudos

Dynamic vector in custom container

Hello.I'm trying to create custom container with any number of elements.I created custom container which contains Scrollable Container and List Layout.I want to dynamically add elements to List Layout. Elements are simple containers which contains te...

Example codes give error.

Hi,When I want to run a touchgfx example (of demo) in designer, compiler give me error like follows.Run Simulator Generate Done Generate Assets make -f simulator/gcc/Makefile assets -j8 cannot load such file -- lib/emi...

The button pressed animation is displayed but the callback is not executed every time the button is clicked

Hi everyone,I am a student and I am working on a project involving an STM32f429ZI and a 7inch touch display.It's the first time I work with displays, I am trying to create a GUI using touchgfx.I have been working on it for a week now and so far I man...

Touftoufe by Associate II
  • 2125 Views
  • 4 replies
  • 0 kudos