STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

I have purchase set STM32H750B-DK, currently i am practice to use toughgfx function, it work well under simulation mode, and i use STMCubeIDE to Compile is ok, no error, when download to STM32H750B-DK. but when download, encounter error below.

I have purchase one set STM32H750B-DK, currently i am practice to use toughgfx function, it work well under simulation mode, and i use STMCubeIDE compile is ok , when download to STM32H750B-DK, encounter error below. appreciate you all able advise.Er...

KLau.1 by Associate II
  • 1793 Views
  • 5 replies
  • 0 kudos

STM32F439 to interface DCMI and TFT Display

Hi Team,I am planning to use STM32F439 Controller and want to interface DCMI and TFT Display ! When i enable both DCMI and TFT Display in STM32CubeIDE, it is giving an error ! Could understand that there is conflict with some pins !Can you please sug...

MPodh.2 by Associate
  • 1295 Views
  • 1 replies
  • 0 kudos

Resolved! error: 'OSWrappers' has not been declared

Hi everyone,​STM32CubeIDE 1.3.032F746-Dicovery​In the above environment, I chose TouchGFX as an additional software and added graphics.And I created a simple GUI for testing by opening the file in the created TouchGFX directory.And when compiling, th...

lsoon by Associate
  • 6627 Views
  • 12 replies
  • 0 kudos