STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Two devices on i2c and TouchGFX

Hello!I have touchscreen on i2c1, which is driven by TouchGFX.Also I have another i2c device on i2c1.If I ty to work with this device after MX_TouchGFX_Init(); - i2c bus is always busy.....How to fix?

EEuge by Senior
  • 875 Views
  • 0 replies
  • 0 kudos

How do I display a Text on TouchGFX?

Stm32f469i_Discovery uses TouchFGX to create a reservation program.I want to show the reservation details on the screen according to the date.The variable for the day of the week is day_value. Mon : 0x01Tue : 0x02Wed : 0x04Thu : 0x08Fri : 0x10Sat : 0...

PKunK.1 by Associate III
  • 1113 Views
  • 1 replies
  • 0 kudos

How to add a font from TouchGFX?

I am using TouchGFX.There is a font that you need during the design of the screen, so I want to know how to add a font.In the picture above, you can see many fonts, and all I want is to add a new font to the font list.The font I am trying to add is K...

0693W000006HdbOQAS.png
PKunK.1 by Associate III
  • 2162 Views
  • 1 replies
  • 0 kudos

Screen tearing in a fixed area, how to avoid it.

The screen tearing issue is as below. It looks always appear in the right area:​The screen is FMC16 bit parallel port, and the parameter is as below:And the screen has TE signal, the TE Interrupt function is an below: void TouchGFX_TickHandler(uin...

0693W000006GwEqQAK.gif 0693W000006GwKFQA0.png
Wrend.1 by Senior
  • 4314 Views
  • 6 replies
  • 0 kudos

greyscale/ color spectrogram plot

Hello Touch GFX Guys,Our application require to plot spectrogram using Touch GFX instead of simple XY-plot.Could you please provide hints or simple example how to do so...Thank you very much for all your support.Regards,I.

IB.1 by Associate III
  • 766 Views
  • 0 replies
  • 0 kudos

Resolved! Can I change the "CAPACITY" of an instance of "GraphScroll" in runtime after its initialization ?

My instance is created in the base file as follows:touchgfx::GraphScroll<50> BlueGraph;And I need to change the capacity of this graph from 50 to 100 to have the line smoother when some event is triggered. Is is possible to change that capacity after...

AGama.1 by Associate II
  • 1648 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.