User Activity

I am working on a project that needs to integrate a 240x240-round display. The display uses a GC9A01A driver, and the host communicates with the driver through an 8-bit 8080 parallel interface. The display vendor provided this interface for communica...
I was working in an application where i need to transmit data from STM32h753 to PC. For this application i used USART1 which is connected to ST-Link. Everything was working fine and suddenly STM32H753 stopped transmitting the data. Even after resetti...
The board was working fine and then after some time i tried to connect again to flash via CUBE IDE but it didn't connect. I am getting the following error when i try to connect using STM32 CUBE PROGRAMMER.i am able to get EVA_H757XI mass storage when...
I am working on a custom LCD project using STM32h753 Eval 2. Currently i dont have a tremendous knowledge in LCD. I tried to follow the example codes and some tutorial but not able to make it work. can you suggest any resource or steps to get started...