STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

How to interface multiple buttons (custom keypad with 12 keys) with touchGFX on a STM32h743bi (320x240) custom board?

Hi Team,as shown above image, I need to implement custom keyboard through hardware buttons,example if press first button at one time 'A' should display, if press continuous two times 'B' should display ,and .i need to display every button values ...

0693W000008vsXFQAY.png
HR M.1 by Associate II
  • 1710 Views
  • 3 replies
  • 0 kudos

Resolved! Variables from Screen1ViewBase are not accessible from Screen1View. I get "VariableName" was not declared in this scope.

I have a variable declare in protected area of the Screen1ViewBase Class: "touchgfx::IconButtonStyle< touchgfx::ClickButtonTrigger > BlinkyAlertIcon;" and I want to use this variable in Screen1View which is publicly derived from Screen1ViewBase. I re...

CStir.1 by Associate III
  • 3309 Views
  • 6 replies
  • 1 kudos

Is freertos Preemtion for touchgfx?

Hi,I have a project for STM32L4R9AI and I have analog and digital clock screens. When I set configUSE_PREEMPTION to 0 my code is stuck. Some tasks are working but my_clock_task and model tick doesnt work. If I set configUSE_PREEMPTION to 1 , every...

Epamuk by Associate III
  • 829 Views
  • 0 replies
  • 0 kudos

Resolved! Custom Widget - Draw function "interrupted"

I followed the Tutorial for the QR Code. It works when you draw just one custom widget. But when i add the same custom widget serveral times in the same Screen or in a custom Container, the code is not able to draw all the custom widgets, it seems th...

GPa.1 by Associate III
  • 3070 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.