STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! I can't access to model from one concrete view.

Hi allFirst of all I'm working with STM32F469I-DISCO board and I'm using TouchGFX Designer- 4.15.0.I have the next problemMy application have 4 different screens, I'm storing in the model general information, and I can access to it without any proble...

Facing issue to interface LCD with stm32f407ve

Hi,I am using STM32F407, trying to interface LCD 16x2 to display sensor data on it.using same code with 8bit mode, I am able to see data on lcd, but when I am trying to use LCD with 4-bit then its not working.. attaching code stm32f4xx_hal.h is attac...

Swagh.1 by Associate
  • 1594 Views
  • 0 replies
  • 0 kudos

Touch GFX 'Status Bar' at Top of all views

Hi, I want to know how to implement a 'status bar' type view that is at the top of all views, that contains things like battery level etc. similar to that found in something like Android or iOS.In the touch GFX documentation it mentions it briefly bu...

savvn001 by Associate II
  • 2382 Views
  • 3 replies
  • 1 kudos

Hello to everyone. I am working with STM32F429 mcu on Touchgfx. I am using a 7inch screen. I am using W25Q128 external flash. Couldn't integrate with Touchgfx. I could not integrate the MB1642BDataReader library in the STM32G0 example into STM32F429.

Hello to everyone. I am working with STM32F429 mcu on Touchgfx. I have successfully run the Touchgfx. I am using a 7inch screen and sending images line by line with DMA. I want to use an external flash as I have too many images to use. I am using W25...

MKoca.1 by Senior
  • 1241 Views
  • 1 replies
  • 0 kudos

4-lane MIPI with STM32F769 Disco

Hi Everyone.I have plan to develop custom board based on kit STM32F769 Disco.TFTLCD I use in this project is 4-lane MIPI (https://focuslcds.com/content/E70RA-I-MW1530-C_Spec.pdf)But as we know STM32f769 Disco only have 2-lane MIPI.So I'm wondering wh...

HAnh by Associate III
  • 3103 Views
  • 4 replies
  • 0 kudos

Resolved! .bdf fonts not working?

Documentation claims:The Font Converter accepts   TrueType (.ttf) OpenType (.otf) Glyph Bitmap Distribution Format (.bdf).I tried to use fonts from:https://github.com/farsil/ibmfontsI put fonts into folder: myproject\TouchGFX\assets\fontsAfter restar...

Tuoman by Senior II
  • 3980 Views
  • 9 replies
  • 0 kudos

How to interface multiple buttons (custom keypad with 12 keys) with touchGFX on a STM32h743bi (320x240) custom board?

Hi Team,as shown above image, I need to implement custom keyboard through hardware buttons,example if press first button at one time 'A' should display, if press continuous two times 'B' should display ,and .i need to display every button values ...

0693W000008vsXFQAY.png
HR M.1 by Associate II
  • 1693 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.