STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! STM32446E-EVA DCMI

Good morning.I am using the STM32446E-EVA board.I want to read data about video from CAMERA through serialI am not sure where it is because it is the DMA part.In order to read CAMERA data, which function part can we know by reading the value in part?...

LSang.11 by Associate II
  • 1334 Views
  • 1 replies
  • 0 kudos

The LCD refresh rate on H7 slower than F4

I use FMC for both H745ZI and F427ZI. I already configured all cores to run at the same clock (168Mhz), but write buffer to F4 seen faster than in H7.Anyone can help me solve this issue? I have included clip at: https://drive.google.com/file/d/15hbrx...

HNguy.21 by Associate II
  • 2754 Views
  • 6 replies
  • 0 kudos

1-Kbyte boundary cross problem, LTDC 1k Boundary

Hello,We are struggling to implement the 1k boundary when reading/writing to a frame buffer i.e. to avoid read operation being split into single accessesHow to do this is described in the application note here:https://www.st.com/resource/en/applicati...

VSimu.1 by Associate III
  • 931 Views
  • 0 replies
  • 0 kudos

Resolved! Are there any samples code for USB Host Application?

Hi Folks,I am trying to explore the USB Host feature for STM32 can offer, I am using STM32F769I-Discovery kit for prototyping. I was trying to find any template for reference on TouchGFX Designer default templates but could not find.Can someone help...

BParh.1 by Senior III
  • 974 Views
  • 1 replies
  • 0 kudos

Resolved! Can not show Image in DSI video mode

(sorry for my bad English)​Hi, My project is base on STM32F469 ,LCD use DSI video mode.Now I can show pixels in TouchGFX box , but can not show images.​Touchgfx project with images:​display like this:​touchgfx project with image&pixel:​display like t...

0693W00000AMdJWQA1.jpg 0693W00000AMcnBQAT.jpg 0693W00000AMdNKQA1.jpg 0693W00000AMdPsQAL.jpg
Zbobo.1 by Associate III
  • 2653 Views
  • 7 replies
  • 0 kudos