STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

How to input chinese characters?

Hello,I know it's not directly related to touchgfx but I thought someone out here could be able to help me and that it could interest others as well. I'm looking for a way to input chinese characters through a conventional qwerty keyboard. Searching ...

GMeur by Senior II
  • 3047 Views
  • 2 replies
  • 0 kudos

Hello, I try to understand how the stm32f469i discovery main loop works with Touchgfx . I've generated a project with Touchgfx and modify it with stm32cubeIde. When I enter in the project there is a task call TouchGFX_Task generated by touchgfx.

I use FreeRtos. I know that the main loop is starting when the function TouchgfxProcess. But I don't know where this function is called. I think it's when the oskernelStart is called but I didn't find where. Could you give me some explanations ?Than...

ECoud.1 by Associate III
  • 3298 Views
  • 6 replies
  • 1 kudos

Resolved! RTC with FreeRTOS and TouchGFX

Hello everybody!Have asked this as a comment in another thread (https://community.st.com/s/question/0D50X0000BvkqIZSQY/inexplicably-slow-rtc?t=1622663635692), but decided to make a separate question in this group.​So far I was able to run STM32H743 (...

ktrofimo by Senior III
  • 4994 Views
  • 9 replies
  • 0 kudos

STM32L4R5Zi Nucleo and ILI9488 SPI based TFT

Hi,I am working on the ili9488 spi based display screen with touch using stm32l4r5zi nucleo kit.After doing number of development it was unable to get start, I get that is my lcd was damaged or already it was faulty.I request to all to share, few run...

SSing.10 by Associate II
  • 990 Views
  • 0 replies
  • 0 kudos

Crash in TouchGFX during initialization

Hi,I am using TouchGFX into a custom board with STM32L476 and simple display with RA6963 driver. Yeah, I know, is too much the TouchGFX for this project.Anyway, I crated the project, I added the low-level driver as suggested here: https://support.tou...

0693W00000BaPckQAF.png
MGiam.1 by Associate II
  • 806 Views
  • 0 replies
  • 0 kudos

Why main.cpp file show hide in STM32CubeIDE?

Hai....,I am using STM32F746IG custom board and 7Inch Display STM32CubeIDE1.6.0 and TouchGFX4.16.0 After upload the code Display show four colors see bellow. In project ..../TouchGFX/simulator/main.cpp show hide and cross symbol image attached bell...

0693W00000BaNX4QAN.jpg 0693W00000BaNe5QAF.jpg
GMano.1 by Associate II
  • 1058 Views
  • 1 replies
  • 0 kudos