STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Cannot enable JPEG decode with DMA on STM32F76xx

Hello,I am currently trying to play a video using the JPEG decoder on a STM32F76xx chip.Right now, I can play a video with HAL_JPEG_Decode in polling mode, but the it takes too long (~100ms) and the FPS is low.My objective, is to use HAL_JPEG_Decode_...

GN.1 by Associate
  • 931 Views
  • 0 replies
  • 0 kudos

TOUCHGFX WILDCARD RANGE ISSUE

Hey Team,Following the examples online , the wildcard range prevents me from inputting 0-120.I've also tried doing 0,120. that lets me input the value , generate the code but not actually show up on the screen

0693W00000BagjxQAB.png
AndreasPA by Associate III
  • 1574 Views
  • 2 replies
  • 0 kudos

Read languages ​​from unmapped SPI flash memory

Hello,I am creating a low cost application with 320x240 LCD and ILI9341 controller.I store all language strings in the unmapped SPI external flash memory by loading the .bin files of each language.Unfortunately I can't see anything on the screen, I s...

0693W00000BadreQAB.png
cb.7 by Associate III
  • 1252 Views
  • 1 replies
  • 0 kudos

[Question] How to configure cubeMX for touchgfx and supplemental touchscreen MB1315A on a STM32L4R9I-EVAL?

Hi,I'm absolutely failing to deploy a successful touchGFX UI on the MB1315A . I can get a touchgfx example deployed on the onboard 390x390 LCD. However, in order to deploy to alternative screens, the documentation says to go through CubeMX.And so I w...

Frebreezy by Associate II
  • 2914 Views
  • 3 replies
  • 0 kudos

How to setup the cache to use Dynamic bitmap ?

Hello everyone,I'm currently developing a project using TouchGFX on a custom board with a STM32F469II and a 1024x600 screen in RGB interface.Right now, I'm trying to add a SD card to the system so that eventually I'll be able to print pictures from i...

TDele.1 by Associate III
  • 3709 Views
  • 8 replies
  • 0 kudos

TouchGFX gray 4 to RGB565

I'm using TouchGfx in Gray 4 mode. I have read the GFX documentation and I can't find the answer. I can't figure out how the data is stored in RAM. Consequently, I need to convert this Gray 4 to RGB565 to my FMC 16bit 8080 TFT-LCD. Any ideas how to d...

KRega.1 by Associate II
  • 1690 Views
  • 3 replies
  • 0 kudos

How to copy the font and image section to binary file?

I am trying using NAND flash to storage the setions, but don`t know how to dump these sections to a binary file, https://support.touchgfx.com/docs/development/scenarios/using-non-memory-mapped-flash shows command "arm-none-eabi-objcopy.exe --dump-se...

JJ.Lin by Associate III
  • 1204 Views
  • 1 replies
  • 0 kudos