cancel
Showing results for 
Search instead for 
Did you mean: 

800*480 LCD CUBE MX setting

JLee.37
Associate II

I would like to use a 24bit 800*480 LCD.

I ask if the value set in CUBE MX is correct.

Please help.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Khouloud ZEMMELI
ST Employee

Hello @JLee.37​ 

Welcome to ST community :)

In case you would use the 24 bits with 800*480 LCD size, as you have configured first, choose the Display type (24 Bits) and set the Horizontal Active width to 800 pixels and the Vertical Active Width to 480 pixels under Parameter settings.

You can also refer to Examples in your repository and under the Example Selector (in CubeMX).

Hope my answer helped you, when your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Thanks for your contribution, Khouloud

View solution in original post

2 REPLIES 2
Khouloud ZEMMELI
ST Employee

Hello @JLee.37​ 

Welcome to ST community :)

In case you would use the 24 bits with 800*480 LCD size, as you have configured first, choose the Display type (24 Bits) and set the Horizontal Active width to 800 pixels and the Vertical Active Width to 480 pixels under Parameter settings.

You can also refer to Examples in your repository and under the Example Selector (in CubeMX).

Hope my answer helped you, when your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Thanks for your contribution, Khouloud

JLee.37
Associate II

​Thank you for answer.

I'm using STM32F429BIT, where can I get the example 800*480 example file?