STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Bitmap database not initialized

I have a TouchGFX project (using V4.17) running on IAR Workbench (V8.42.4), which consists of some on-screen images defined by the GUI in the *screenbase files and some dynamic ones defined and controlled by user code. If I comment out the user-defin...

0693W00000GWzC1QAL.png
Water123 by Associate II
  • 664 Views
  • 0 replies
  • 0 kudos

Image Quality Problem at AT25SF128A External Flash

Hi,I use flash memory ( at25sf128) in my project and I can read data from flash correctly, I checked it . Also I checked the configuration of quad in out fast read command. However, The images do not have correct view on LCD. Have you ever had this p...

0693W00000GWSA7QAP.jpg 0693W00000GWtG7QAL.jpg
NDura.16 by Associate II
  • 915 Views
  • 0 replies
  • 0 kudos

[Dynamic Graph] How to add data points with x value?

I want to draw a graph, and what I expect is that the data points on the left are dense and the data points on the right are sparse. But I only found AbstractDataGraphWithY, a class that ignores x, is there any similar class that does not ignore x ca...

Zwei.9 by Associate III
  • 768 Views
  • 0 replies
  • 0 kudos

Include files Not Accessed in IDE File Search

In example projects created from within TouchGFX Designer and imported into a STM32CubeIDE workspace, the user gui folder only contains .cpp files. The example project itself (represented by the presence .project and .cproject files) is located in th...

0693W00000GWh6tQAD.png 0693W00000GWh6yQAD.png 0693W00000GWh73QAD.png 0693W00000GWh78QAD.png
DSwea.1 by Associate III
  • 1054 Views
  • 3 replies
  • 1 kudos