cancel
Showing results for 
Search instead for 
Did you mean: 

How to create TouchGfx project for STM32H745i ?

limit_SKY
Associate II

In the default MCU selection tool in touchgfx there is no STM32H745 configuration. I want to use 745 for my project and use touchgfx.

I plan to migrate from either 750 or 743 or 735 to h745. I started h750 and I changed startup files, ld flash files and all stm32h745i_discovery_* files. I also change the .project and .cproject files. But I could not make project work. There are tons of compile errors.

Which board is the most close to the STM32H745, and which files should I change to make the touchgfx project work on this board. Is there a guide?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
CN.1
Associate II

Same question here