STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

2.8'' ILI9341 SPI LCD and XPT2046 Touch Controller

I'm trying to integrate the display in question with TGX 4.13. This is the LCD module.I developed the drivers for both display and touch, configured the project and trying to follow what is reported in the documentation at this link (spi scenarios fo...

ALomb by Senior
  • 11979 Views
  • 25 replies
  • 0 kudos

Resolved! About scrolllist.

How to solve the problem of slow scrolllist sliding process, when the item template is too complicated(Template size :710*35,contains 4 textAreas�?2 bitmaps 5 boxs,Scrolllist size :710*350).The simulator is very nice,but H7 board is not smooth.

Zwei.9 by Associate III
  • 1838 Views
  • 3 replies
  • 0 kudos

TouchGFX Designer Feature Request

The custom containers feature is obviously a very useful, and I might add, indispensable tool. However, it's application is somewhat hampered by the inability to see the name of the underlying component once the component is added to a screen, and th...

0693W00000HpvSRQAZ.png
DSwea.1 by Associate III
  • 2227 Views
  • 5 replies
  • 1 kudos

How to debug 071RB touchgfx demo code on IAR IDE?

Hello,I am trying to debug Nucleo_017RB touchgfx demo code with IAR IDE.After build on IAR, I tried to debug Nucleo071RB but failed at ext-flash programming stage. I guess IAR(v9.10.2) do not have right flashloader file.So when I tried to debug it wi...

Tiel by Associate II
  • 1077 Views
  • 3 replies
  • 0 kudos

Hello, I download the material available in the example about workshop2020 touchFX in youtube link: https://www.youtube.com/watch?v=rYrRjXyAYvs Compiling with STCubeIDE the projects generates some error.

I unzip the project STM32H7BWorkshop2020_labs12 i open the touchGFX project with new version 4.17. I apply  the advice suggested to convert project from vers 4.13 to 4.17 e regenerate the code.then i open STmCUBE IDE but when i built the project it g...

0693W00000FDZ8LQAX.png
EMir.1 by Associate II
  • 5769 Views
  • 13 replies
  • 0 kudos

Black screen after running target

Hello :)I was doing setup from that tutorial on STM32F7508-DK:https://www.youtube.com/watch?v=2LQpaz44Ug4&ab_channel=STMicroelectronicsI replaced ADC with I2C and make callback from Master Receive instead of ADC Callback.void HAL_I2C_MasterRxCpltCall...

0693W00000Hq6odQAB.png
AWe.1 by Associate II
  • 1810 Views
  • 3 replies
  • 0 kudos