STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

ST product recommendations (cameras/wifi)

I'm looking for some processors to achieve a couple tasks. First, I would like to get input from two cameras. The interface isn't important, I will find the cameras based on the processor. But then I want to also be able to send that video stream ...

Syscall _exit() on string manipulation

I am using TGX v4.16.1 and CubeIDE v1.8.0. My hardware platform is the STM32429 Eval board.The code for the hardware backend was autogenerated from either TGX Designer or CubeMx (I do not recall which one at this point).My issue is that the applicati...

0693W00000HqnzAQAR.png 0693W00000Hqnz0QAB.png
CPaye.1 by Associate III
  • 2289 Views
  • 3 replies
  • 0 kudos

I'm working on stm32f469 discovery board for GUI application , using stm32cubemx 5.4 and graphics framework stemWin, where I want to display integers from 1 to 5, my delay function is not working I guess, only 1st value 1 is displaying on the screen.

This is the application code, which I'm writing on GUI_App.c ,for (uint8_t i = 1; i < 5; i++) { GUI_DispDecAt(i, (LCD_GetXSize() - 150) / 2, (LCD_GetYSize() - 20) / 2, 1); GUI_Delay(1000);}can anyone please guide me through this, thanks in advan...

SSabo.1 by Associate
  • 1269 Views
  • 1 replies
  • 0 kudos

WM_TIMER stops firing after some time in stemwin

I am using stm32h747 with Microsoft Azure. I am using a LCD Screen with LTDC controller and am using stemwin for GUI. I have multiple UI pages. In every page, I am getting the time from internal RTC of MCU and displaying it on the screen. I am updati...

SLuit.1 by Associate III
  • 831 Views
  • 0 replies
  • 0 kudos

how move page like iphone by Swipe container

First, I'm japanese, so my English is not good. sorry.​Please teach how move page like iphone by Swipe container.I made touchGFX project using Swipe container.The page have many button widget.I try swipe with pushing button widget, but The page don't...

Htera.1 by Associate II
  • 1661 Views
  • 2 replies
  • 0 kudos