STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

How to make STM32L476VGTx use GUIBuilder?

HelloI want to know how to make The STM32L476VGTx can use GUIBuilder to design a custom GUI to display on an LCD screen.I want to know if it is possible or not. or is there any way(Actually my project is a ST25R3916 board that uses an STM32L476VGTx M...

mchal.11 by Associate
  • 1153 Views
  • 1 replies
  • 0 kudos

D-Cache failed again?

While heavy updating customized DynamicGraph after some time (from 10 minutes to more then an hour) application goes to HardFault.Investigation shows that problem always happens inside TouchGFX library function CWRUtil::Q5 indexToScreenXQ5( const Abs...

ktrofimo by Senior III
  • 1799 Views
  • 3 replies
  • 0 kudos

Resolved! How to run parts of the program from external QSPI

I would to use the cheap STM32F750N8-DISCO evaluation board to run a ETH/I2C/SPI/IR/encoder/touch-screen application but the 64K of flash is very little for my program.Now my program run a STM32F746G-DISCO with 1Mbit of flash and it use about 450K.I ...

DSI Long write stops sending data.

I'm using a custom board with an STM32F469, a display with an ILI9488 320X480, and a frame buffer of 1X480. This frame buffer should fill a line of data.When I send the packet using a DSI Long write, only part of the line is filled up with the data I...

C.East2 by Associate III
  • 1558 Views
  • 1 replies
  • 1 kudos

Can the STM32H743 emulate the performance of the STM32F469?

Hello,Using the 180MHz clock on the STM32H743, will the performance for the SPI (using ILI9341 display) and LTDC functions be similar to those obtained on the STM32F469?​​I would like to try this STM32F469 in place of the STM32F407. But I don't have ...

by Not applicable
  • 1859 Views
  • 5 replies
  • 0 kudos