Skip to main content
IHei?
Visitor II
October 14, 2021
Solved

TouchGFX - SPI - PartialBuffer: Can I set the Position/Width/Height to a multiple of 2?

  • October 14, 2021
  • 2 replies
  • 1328 views

Hello,

I have a STM32F723 Application with TouchGFX (4.16.1) Graphics over SPI and a Display with RM69330 Controler (454x454x2Bpp).

I use PartitialBuffer Configuration, because internal RAM is too small for whole Framebuffer. I've implemented the Transmit Function ("touchgfxDisplayDriverTransmitBlock( uint8_t* pixels, uint16_t x, uint16_t y, uint16_t w, uint16_t h)") where I set Position Rectangle in Display Controler and write Pixels to the Display. That works fine if x/y/w/h are a multiple of 2 otherwise it looks weired.

Problem is: In RM69330 DataSheet it says that Column and Row Startaddress and Width / Height "must can be divisible by 2".

Question: Is there any way to tell TouchGFX to only supply framebuffer parts with x/y/w/h as a multiple of 2? Or is there any other Known solution?

This topic has been closed for replies.
Best answer by Alexandre RENOUX

Hello IHei?,

This problem can happen and we discovered this is a common limitation for several SPI displays.

To fix it, you have to modify FrontendApplication.hpp and .cpp as below :

FrontendApplication.hpp

virtual void draw(Rect& rect);

FrontendApplication.cpp

void FrontendApplication::draw(Rect& rect)
{
 if (drawCacheEnabled)
 {
 Rect even(rect);
 //ensure start x is even number, or move left
 if (even.x&1)
 {
 even.x--;
 even.width++;
 }
 //ensure width is even number of pixels
 even.width = (even.width+1)&~0x01;
 
 //ensure start y is even number, or move up
 if (even.y&1)
 {
 even.y--;
 even.height++;
 }
 //ensure height is even number of pixels
 even.height = (even.height+1)&~0x01;
 
 Application::draw(even);
 }
 else
 {
 Application::draw(rect);
 }
}

You basically overwrite the draw function to ensure even numbers for the rectangle to draw.

When your question is answered, please close this topic by choosing Select as Best.

/Alexandre

2 replies

MM..1
Super User
October 14, 2021

Maybe you can in your transmit function extend x,y,w,h to multiple 2 with read data from display , but yes this is more overhead as send only.

Alexandre RENOUX
Alexandre RENOUXBest answer
Visitor II
October 19, 2021

Hello IHei?,

This problem can happen and we discovered this is a common limitation for several SPI displays.

To fix it, you have to modify FrontendApplication.hpp and .cpp as below :

FrontendApplication.hpp

virtual void draw(Rect& rect);

FrontendApplication.cpp

void FrontendApplication::draw(Rect& rect)
{
 if (drawCacheEnabled)
 {
 Rect even(rect);
 //ensure start x is even number, or move left
 if (even.x&1)
 {
 even.x--;
 even.width++;
 }
 //ensure width is even number of pixels
 even.width = (even.width+1)&~0x01;
 
 //ensure start y is even number, or move up
 if (even.y&1)
 {
 even.y--;
 even.height++;
 }
 //ensure height is even number of pixels
 even.height = (even.height+1)&~0x01;
 
 Application::draw(even);
 }
 else
 {
 Application::draw(rect);
 }
}

You basically overwrite the draw function to ensure even numbers for the rectangle to draw.

When your question is answered, please close this topic by choosing Select as Best.

/Alexandre