STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Can't write on external flash w25q128jv

I am trying to initialize my W25Q128jv External Flash in my project, but I am not able to write on it and I think it could be because of the Memory Mapping Mode but I really don't know. For this project I will need my QUADSPI when I will add TouchGFX...

Gpapa.1 by Associate
  • 3476 Views
  • 3 replies
  • 0 kudos

Resolved! Example for Scroll Wheel with Text-Group Strings?

Hello,i try to create a scroll wheel with some texts as items.So i created the container and the highlighted container.Then i created a Group in the Texts "Scrollwheelgroup" with 6 Resources inside.FristResource, SecondResource, ......I want to show ...

Resolved! how does the stm32u5 work with lcd

There's a dev board with a lcd, but the U5 doesn't seem to have support for the same LTDC that that chips like stm32L4 or stm32F7 does.https://www.st.com/content/st_com/en/products/evaluation-tools/product-evaluation-tools/mcu-mpu-eval-tools/stm32-mc...

Badam.17 by Associate II
  • 3350 Views
  • 2 replies
  • 0 kudos

Resolved! [SOLVED] After the instruction MX_TouchGFX_Init(), FATFS methods do not work as wanted (STM32F469I-DISCO)

When I'm using TOUCHGFX and FATFS together, I can create/write/read a file in my SD only if I do it before "MX_TouchGFX_Init();"f_mount(&SDFatFS, (TCHAR const*)SDPath, 0);f_open(&SDFile, "DIO.TXT", FA_CREATE_ALWAYS | FA_WRITE); //with TGFX this one g...

0693W00000KdYSvQAN.png 0693W00000KdYSgQAN.png 0693W00000KdaPPQAZ.png
William F by Associate II
  • 1378 Views
  • 1 replies
  • 0 kudos

STM32L4 and DCMI with 24bpp

Hi,I´ve done a lot of reading and testing...For some reason, its stated in both the datasheet and the DCMI application note that 24 bit per pixel formats are not supported. Trying to understand why...The DCMI is "stupid" in the sense that we only tel...

AJans.3 by Associate II
  • 1159 Views
  • 1 replies
  • 0 kudos

How to add GPIO bindings to my VS Application?

I made a test project for my discovery board with TouchGFX.I needed the UI to react for a pin state change.I've seen tutorials, where a GPIO accessing function was added to the `main.c` file. Then it could be added as `extern "C"` from `Model.cpp` fi...

HTD by Senior III
  • 2798 Views
  • 5 replies
  • 0 kudos