STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

How to set the slider position from code.

I have been able to get the slider position using a callback function but need to set the slider position when the page is shown from a stored value. I don't need continuous updates only when page is activated.Thanks

radioman by Associate II
  • 4298 Views
  • 7 replies
  • 0 kudos

LCD HD44780 interface problems with Nucleo board

Hello all members,I am interfacing LCD module in 8bit mode to STM32F446RE Nucleo board the connections are as below:The pin connections(if unclear in diagram):Control pins:RS-->PB0RW-->PB1E-->PB38bit data pins LCD:D0-D7-->PC0-PC7Program Lcd.c: #inclu...

0693W00000Lz4htQAB.png
dk.2 by Associate II
  • 4703 Views
  • 10 replies
  • 0 kudos

3.5" TFT Display (320x480) with Stm32U5

Hi,For one of our upcoming products, we're planning to use stm32u5 & therefore evaluating the uC for that purpose. It needs to have a 3.5" TFT display and we're wondering if there could be any suggestion from ST's side on that:Since there is no LTDC ...

UKhan.2 by Associate II
  • 2270 Views
  • 1 replies
  • 0 kudos

Resolved! How to drive reused containers?

I'm currently working on my second ever TouchGFX project and keep stumbling upon the same issues as in my first one.I have a battery indicator that I would like to show on (almost) every screen. For this reason I created a container that I can easily...