STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Linker error when building project in VSCode

I'm trying to port TouchGFX to VisualStudio Code + PlatformIO using ZephyrRTOS for the STM32F746-Disco board. To do that, I've just created an example project on TouchGFX Designer 4.17, generated the code, and added the required files manually as sai...

JZumt by Associate II
  • 3758 Views
  • 4 replies
  • 0 kudos

TouchGFX compatibility with ChibiOS

Hi,Doing some research for development of a smartwatch like product and was trying to figure out if TouchGFX was compatible with ChibiOS.It seems like it should be possible, with the docs saying that any CMIS compliant OS is supported, however I want...

DOkaz.1 by Associate II
  • 2353 Views
  • 5 replies
  • 0 kudos

Custom Touch GFX

Hi Community,I have stored framebuffer in Internal RAM and assets in QSPI Nor Flash. I am not getting the desired display output.

Vins by Senior
  • 990 Views
  • 1 replies
  • 0 kudos

Synchronizing LCD output with Tearing-Pin information?

Hi,I am using the ST32F412G discovery board, which has a 240x240 LCD attached to the controller using the FSMC interface. At the moment I am using the driver from the board support package and drawing works fine.I will be drawing moving shapes to the...

MLa.3 by Associate II
  • 3150 Views
  • 1 replies
  • 0 kudos