STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Moving the slider Knob without Touch.

Hi...I have configure the slider Widget using TOUCHGFX & it is working fine with Touch. But the want to Configure the slider without touch i.e., When I give some Data through Usart , according to that data the slider knob has to move (Without touchin...

PM.5 by Associate III
  • 1922 Views
  • 3 replies
  • 0 kudos

Resolved! Images aren't rendered properly on screen

Hi,Here is how my widgets are currently rendered on my ST32F769I-discovery board. I know the problem is related to the external flash because the only image saved in the internal flash is displayed properly but I don't know exactly where the problem ...

0690X000009Z2NJQA0.jpg
GMeur by Senior II
  • 3559 Views
  • 7 replies
  • 0 kudos

how do you combine stm32f446 and gfx01m1?

Hi all, I m very new using stm32CubeIDE and TouchGFX.I m trying to interface the two, but when creating a new project on TouchGFX, I am unable to find the stm32f446 Mcu to start my screen design.Am i doing something wrong ?

theo481 by Associate
  • 1164 Views
  • 1 replies
  • 0 kudos

How can I access the model from a custom container

Hi, I have a common custom container that is included in all my views.I need to access a method from the model, usually, in a view, I do this from the presenter, how can I do this in the custom container in a general way without passing the view to t...

How to use standard concurrency support library in simulator (error: 'mutex' in namespace 'std' does not name a type)

Hello,I am getting this compilation error when running simulator:error: 'mutex' in namespace 'std' does not name a typeFrom the informations I had found about this topic, this error is caused by used thread model of MINGW32. MINGW32, which comes toge...

external adc + dcmi

HI theremy pervious post explains the issue https://community.st.com/s/question/0D53W00001lTyoOSAS/read-parallel-cmos-adc-using-nucleoh743zi2after a bit of research I found that I can use the DCMI(digital camera interface) as an input to the ADC bec...

AElta.1 by Associate II
  • 4858 Views
  • 3 replies
  • 0 kudos