cancel
Showing results for 
Search instead for 
Did you mean: 

How to resize a project to a higher resolution.

Amaresh
Associate III

I have made a project for STM32f469I-DISCO ie. 4" 800x480 resolution. How do I resize/convert the entire project which consists of 12+pages and 100+ images and texts to a 5" 1280x720 screen without redesigning it?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
MM..1
Chief III

You can simply reconfig template file edit, but your design stay as is, only new free space add.

Scaling images and objects isnt trivial and is in your hands...

Next question is LCD resolution handle by hw...