User Activity

I am having trouble how to setup the Linux system on the STM32MP1 so that I can use sftp to upload data gathered by the device to an external server.What happens is that once the connection is established it immediately closes again, so there is no t...
Hello,I try to install the distribution package usingrepo init -u https://github.com/STMicroelectronics/oe-manifest.git -b refs/tags/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15as described in the wiki, before that made sure to install all packages...
I am having difficulties activating the EXTI interrupt for a pin in the M4 NVIC.   What I did: Opened STM32CubeMX,selected the board STM32MP157F-DK2,opted to configure all peripherals in their default stateActivate SPI5 in the M4 domain, incl. DMA do...
Dear all, I have successfully implemented the example STM32CubeH7-master\Projects\STM32H747I-DISCO\Examples\JPEG\JPEG_DecodingFromFLASH_DMA with the image file given as C source there.Now I wanted to change the image data, which however was not succe...
Kudos from