Difference between object.setVisible(false) and remove(object)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-04-28 1:20 AM
If user wants to make object invisible, which method is the most efficient, e.g. in terms of performance or memory usage?
Generally, in which cases should use setVisible true/false vs. add/remove?
Is it so that the only difference is that remove/add modifies drawing order, but otherwise they are equal? (I.e. performance to draw removed or invisible objects are both neglible)
In that case add/remove should only be called in init (or if drawing order must be changed), and setVisible afterwards...
- Labels:
-
TouchGFX
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-04-30 11:49 PM
Hello, Tuoman.
> Is it so that the only difference is that remove/add modifies drawing order, but otherwise they are equal?
No. It differs in several points. I will write my understanding.
`setVisible()` is a function to show a instance based on `Drawable` class.
- There are no effect to memory usage because `setVisible()` work on only its visibility.
`remove()` is a function to delete a instance based on `Drawable` class for future rendering.
- `remove()` is not a function of `Drawable` but of `Container` (Screen class has its own "root container". See here).
- If a instance based on `Drawable` is removed from `Container`, it result in being removed from memory.
- When a user call `add()` for redrawing some widgets, TouchGFX might be acquire a new memory region for those widgets.
So I think as follows.
- If you switch visibility of a component repeatedly, it is good to use `setVisible()`.
- If you delete some instance and never use it, it is good to use `remove()`.