STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Word warp issue with multi-line texts (3 lines)

Hi,I am using word wrap with Text Area component:textArea.setWideTextAction(WIDE_TEXT_WORDWRAP);My texts are usually so long that they need to be wrapped to 3 lines. I have seen no issue with the first wrap (between line 1 and 2), but the second warp...

PWagn.1 by Associate II
  • 3148 Views
  • 5 replies
  • 0 kudos

Resolved! Hello, i am tring to display some word on my LCD connected by means I2C drive (LCM1602) without result. I have no error and the LCD is always on but no word apper. I think that the issue is the address to put in: #define DEVICE_ADDR (0x4E << 1)

On data scheet of device (PCF8574T mounted on LCM1602) the addres is 0100 1110=4E but the program still doesn't show me any letter on LCD. Where is wrong? I cheked many times the pin and them are right. Same thing on Cube IDE.

SMusc.1 by Senior
  • 4254 Views
  • 5 replies
  • 0 kudos

DMA2D

Hi, I have initialized 1 layer in 800 * 480 resolution, and I also I have initialized DMA2D for this layer. I got 2 problems:1- when it loads my logo , I see some lines which I can't understand how they come!! for this: some horizontal lines appeared...

nsabo.1 by Associate II
  • 1234 Views
  • 1 replies
  • 0 kudos

How to store Video (.obj and .bin) files in external memory as they have stored in Touch GFX example codes or any generated from Touch GFX designer projects?

Hi Community,How to store Video (.obj and .bin) files in external memory as they have stored in any generated project from Touch GFX designer?Already we stored image data in external memory by using pragma location and linker script. But now I want t...

0693W00000UnZOfQAN.png
Vins by Senior
  • 945 Views
  • 0 replies
  • 0 kudos