2022-05-12 8:13 AM
My software for touchscreen in the board MB1260 D-01 works, but the same software for the revised board MB1260-F723E-D03 does not work! Any idea?
2022-05-12 8:50 AM
Hello
I have heard about some update of the touchscreen controler chip.
so the driver needs to be changed accordingly.
ft6x06 => ft3x67
I don't think it is present in the F7 software package (yet?).
But I know it is in latest L4 package... STM32Cube_FW_L4_V1.17.1\Drivers\BSP\Components
Please check the attached file.
2022-05-12 9:22 AM
So, will the replacing of the driver in the software help with the upgrade? Thanks
2022-05-13 12:53 AM
Hopefully yes.
2022-05-13 10:50 AM
OK will try it! Thanks again!
2022-05-13 10:52 AM
And can you send me the driver files again! I'm not able to open them.
2022-05-16 12:56 AM
The file is still in my previous post.The archive is valid.
Open it with 7zip.