User Activity

I have a custom lcd to drive with STM32L073VBTx's internal lcd driver. Duty cyle is 1/4 and the bias is 1/3. The problem is the common pins are activated sequentially even the LCD's RAM registers are equal to 0. When I activate some bits in LCD's RAM...
Hi everyone,I have stm32L053R8 nucleo64 board. I'm trying to get adc measure in low power run mode. It's not working correctly in Lprun mode but when I try in run mode it's working. In Lprun mode I only get 2 values. Half of the resolution and full o...