STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

STLK Over Current LED 2 blinked

As I am using the STM32H745 board when I attach my external board to the controller the LED2 of the controller starts blinking. As datasheet refer LED2 to STLK Over Current. now my LCD is not working nor is it debugging. but LED2 and LED3 are still b...

SAMIN.1 by Associate III
  • 1855 Views
  • 2 replies
  • 0 kudos

text doesn't change

i simply create a application with a label button, container with two radio button shown belowactually what i want is when i click the button show the container (do it with interaction and virtual function calling)container.setvisible(true)container....

0693W00000WIFCqQAP.png 0693W00000WIFFAQA5.png 0693W00000WIFEvQAP.png
MA.21 by Associate III
  • 2879 Views
  • 4 replies
  • 0 kudos

space character

as i includeUnicode::snprintf(textArea1Buffer, TEXTAREA1_SIZE, "%s%d\n", textArea1Buffer, pda[i]);   //textArea1.invalidate();    textArea1.invalidate();it works when i replace \n with \t show fallback characte(?)what is actually happenalso addwildca...

0693W00000WIOI8QAP.png
MA.21 by Associate III
  • 2407 Views
  • 4 replies
  • 0 kudos

[STemWin]Inconsistent wchar_t size warning on IAR 8.50.1

Hello, When I try to build source codes including STemWin(5.40) library, following warning is shown and display is not work. when I tested at IAR 7.80.4, there was no problem.Warning[Lt009]: Inconsistent wchar_t size       GUIAA_Char4Ext_XBF.o(STemWi...

Tiel by Associate II
  • 1730 Views
  • 1 replies
  • 0 kudos