STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

I get an error when I try to open my 4.18.1 project into 4.19.0: C:/TouchGFX/4.19.0/env/MinGW/msys/1.0/Ruby30-x64/lib/ruby/3.0.0/rubygems/version.rb:214:in `initialize': Malformed version number string - (ArgumentError)

I'm trying to get my 4.16.1 project updated to 4.21.1, but the conversion fails. I then tried installing all the versions in between, and can see that it fails from 4.18.1 to 4.19.0:The full error message: C:/TouchGFX/4.19.0/env/MinGW/msys/1.0/Ruby30...

KKark by Associate II
  • 3435 Views
  • 7 replies
  • 0 kudos

X-CUBE-TouchGFX 4.21.2 is out !

TouchGFX 4.21.2 is now out.Please follow this link to download it.4.21.2 Release details :Release date: March 1st, 2023Bugfixes in TouchGFX Designer:Fixed crash related to interactions.Fixed crash related to deleting texts in search results.Fixed SVG...

STM32F469I-DISCO

Hello, I am very new to STM32 boards. I just purchased an STM32F469I-Disco and have already installed STM32CubeIDE and can connect to the board via STM ST-LINK Utility v4.6.0 and see the blinking LEDs. However, when I power the board, the screen is b...

Shawn1 by Associate
  • 1717 Views
  • 3 replies
  • 0 kudos

FreeMarker template error

Hello all,ST is obviously ignoring problems because i have found few topics about this issue which are two years old. So, during TouchGfx generation from CubeMX i get an errors in TouchGFXGeneratedHAL.cppJava has obviously still have problems with bi...

Eiffel by Senior
  • 3711 Views
  • 8 replies
  • 0 kudos